<< Return to Login Help Menu < See more questions about keyfob access
How do I log in to JOE?
To access JOE using a keyfob, you must have:
- a valid User ID
- a keyfob
- a PIN number for use with the keyfob
Open Internet Explorer, and enter connect.eaton.com in the "Address" field. (Please note that there is no "www" preceding the address.) Once the JOE login screen appears, enter your User ID and click Continue.
Your User ID is the same as your Oracle ID number, left-padded with zeros to a maximum of seven digits, and preceded by an "E". For example: if your Oracle ID is 12345, your User ID would be E0012345. Enter this in the "User ID" field.
On the second login screen, enter your password and click Login.
Your password is a ten-digit number consisting of a 4-digit PIN and the 6 digits displayed on the keyfob. The 6 digits on your keyfob change approximately every 60 seconds. Enter the 4-digit PIN followed by the 6 digits as displayed on the keyfob with no spaces, dashes, or other characters. In case you do not enter the password before the digits displayed on the keyfob change, clear this field and begin again.
It is highly recommended that you memorize your 4-digit PIN. Do not share it with others or write it down on or near your computer or on the keyfob device itself. |